MITSUBISHI ELECTRIC Changes for the Better

Power Train - Engine Machining

  • Knowing an optimal timing to replace tools of machine tools
  • Enhancing traceability to reduce machining defects
  • Improving cycle time and reducing control panel size through space saving by controllers(PLCs/CNCs)
  • Preventing damage to servo motors caused by coolant during machining

Solution overview

Issues Solutions
Knowing an optimal timing to replace tools of machine toolsDiagnose tool wear condition by detecting torque change of each axis.
Enhancing traceability to reduce machining defectsUnitarily manage the data collected by the high-speed data logger module.
Improving cycle time and reducing control panel size through space saving by controllers(PLCs/CNCs)Configure a multiple CPU system by PLC CPUs and CNC CPUs.
Preventing damage to servo motors caused by coolant during machiningEnhance water resistance with IP67 rated servo motors and fanless control panels.

Solution details

Knowing an optimal timing to replace tools of machine tools

Replace tools at an optimal timing by diagnosing tool wear condition and detecting torque change of each axis.

Replace tools at an optimal timing by detecting torque change of each axis and diagnosing wear condition.

CBM (Condition Based Maintenance) finds the peak loads of each tool from past machining data and uses it to predict the number of tool usages. Notifying the operator of the predicted number of tool usages remaining contributes to visualization of tool wear.

Key Points

  • Reduce tool replacement costs by using tools up to their service life.
  • Find the peak loads of each tool from past machining data and use that data to estimate the number of times a tool can be used. Notify the operator of the estimated result.

Enhancing traceability to reduce machining defects

Collect machining data with the high-speed data logger module without creating a ladder program. Realize traceability by automatically sending the data to the FTP server and unitarily managing it.

The high-speed data logger module logs various data in the production process and realizes traceability of the production site by changing settings without stopping the equipment.

CBM (Condition Based Maintenance) finds the peak loads of each tool from past machining data and uses it to predict the number of tool usages. Notifying the operator of the predicted number of tool usages remaining contributes to visualization of tool wear.

Key Points

  • Save logging data in the Unicode/CSV/BIN file formats, and create various materials such as daily reports, ledgers, and reports in an Excel file format.
  • Logging files can be automatically transferred to server computers.

Improving cycle time and reducing control panel size through space saving by controllers (PLCs/CNCs)

Reduce control panel size by installing PLC CPUs and CNC CPUs on the same base unit, incorporating a machining process into a conveyor control process. Shorten cycle time by a Mitsubishi Electric's original CNC-dedicated CPU that reduces high-speed data communication processing time.

A CNC CPU is a multi-CPU CNC supporting MELSEC iQ-R series.

High-accuracy machining with shorter cycle time is achieved by high PLC processing capability, faster optical communication between the CNC CPU and the drive, and shorter processing time between the CNC CPU and the PLC

Key Point

  • CNC CPUs and PLC CPUs are independent, allowing a flexible system configuration according to the production scale and applications.

Preventing damage to servo motors caused by colant during machining

Use IP67 rated servo motors to prevent damage to servo motors caused by coolant. Enhance water resistance with the fanless structure of the control module which enables fanless control panels.

IP67 rated servo motors prevent damage caused by water or dust entering the junction point such as the shaft portion of the motor.

Key Points 

  • Prevent damage caused by coolant with IP67 rated servo motors.
  • Prevent damage caused by mist invasion with fanless control panels.

Product Lineup

Competencies

Our Stories

2026-07-07

NEWThe factory that thinks - turning data into real shop floor performance

Mitsubishi Electric Automotive Czech

EN
Ogledate si video na YouTube
#Automotive#MES interface

2026-07-07

NEWBMS-Driven energy and facility performance

Mitsubishi Electric Automotive Czech

EN
Ogledate si video na YouTube
#Automotive#Mitsubishi Electric Iconics Digital Solutions#GENESIS64#MELSEC iQ-R Series

2024-06-01

Industrial robots as an unusual measuring tool for testing radar sensors

Noffz GmbH

ENDE
#Automotive#Digitalisation#Industrial Robots - MELFA

2023-11-07

E-Motor Production

Renault Group

Ogledate si video na YouTube
#Automotive#Digital Manufacturing#Programmable Controllers MELSEC#Visualization

2018-11-01

Poka Yoke: Error-free manual workstations

Werkstatt Bremen - Martinshof

DE
Ogledate si video na YouTube
#Automotive#Material Handling#Controllers#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA

2012-08-01

Plasma deburring in the automotive supply industry

MW-TEC GmbH & Co. KG

ENDE
#Automotive#Human-Machine Interfaces (HMIs) - GOT#Robots#Controllers

2007-06-13

Robot-assisted Hot-Melt Gluing Station

Otto Kuhlmann GmbH & Co. KG MW-TEC GmbH & Co. KG

ENDE
#Automotive#Robots#Controllers

2007-03-01

Flexible part measurement system for quality control

Schmidtke electronic

ENDE
#Automotive#Robots