MITSUBISHI ELECTRIC Changes for the Better

In this case study…

  • Higher testing accuracy with real-time force control,
  • Improved reliability despite component tolerances and variability,
  • Faster validation through virtual commissioning,
  • Reduced scrap and increased process efficiency,
  • 60% faster application development through AI-enabled automation.

Today's world faces several challenges. One of them is the transformation of the automotive industry. Electrification, connectivity, shared mobility, and autonomous driving are reshaping transportation. In this new reality, high-precision operations require reliable and repeatable processes capable of handling increasingly tighter tolerances. Minebea AccessSolutions designs intelligent solutions ranging from door handles to keyless systems for vehicle access and security. To ensure high-quality standards and increase production efficiency, Minebea AccessSolutions chose to automate a critical testing phase by implementing Mitsubishi Electric industrial robots equipped with an AI-powered force sensor.

The challenge: managing tolerances and variability without compromising quality

Minebea AccessSolutions needed to develop a highly flexible testing and simulation bench capable of accurately replicating human touch by modulating force values, acceleration, and different geometric trajectories. The goal was to implement a solution capable of dynamically adapting to operating conditions while continuously monitoring the applied load to ensure the highest level of process accuracy.

“We need to develop a test and simulation bench flexible enough to simulate human touch with the ability to measure the level of forced applied acceleration and speed values and different trajectories” Francesco Lamanna, Manufacturing Engineering Manager.

The solution: MELFA robots with force sensor technology

To address these requirements, Minebea AccessSolutions chose to use Mitsubishi Electric MELFA series robots, capable of detecting force during assembly, part processing, and testing operations. This enables the robots to perform tasks that require force adjustment and force detection. As a result, the robot does not simply follow a programmed path but actively responds to contact with the component.

The results: a tailor-made, innovative, high-performance solution

The complete integration of the robot and sensor enabled real-time test traceability and management of the entire system directly through the robot software. Integrated AI models also helped reduce and optimize development and commissioning times. The entire process was digitally replicated and tested within the Gemini Virtual Commissioning software environment.

As a result, Minebea Access Solutions managed to achieve: 

  • 60% reduction in development time thanks to artificial intelligence functions,
  • adaptive force control based on user-defined parameters,
  • high execution speed and precision in testing operations with real-time measurement monitoring,
  • completing traceability of position and force data at the moment of contact.

Why it matters?

The implementation of the Mitsubishi Electric solution delivered numerous benefits to Minebea AccessSolutions' production process, including:

  • greater operational reliability,
  • reduced errors caused by tolerances and misalignments,
  • improved process quality and repeatability,
  • reduced scrap and rework,
  • continuous parameter monitoring,
  • increased overall line efficiency.

Thanks to the combination of advanced robotics and force control, Minebea AccessSolutions was able to simultaneously improve productivity and quality while maintaining high operational standards even in the most complex applications.

“The technical team has successfully supported the Minebea Mitsumi group, perfectly interpreting our process needs and proposing innovative, concrete solutions that exceed expectations” Vittorio Giaccone, Head of Divisions – Purchasing.

Discover the solutions behind this case study

Have we sparked your interest? Contact us

0/255
Polja, označena z *, so obvezna.

Our Stories

2026-10-20

NEWRobotics and force sensing for intelligent testing of automotive components

MinebeaAccessSolutions

EN
Ogledate si video na YouTube
#MELSOFT Gemini 3D Simulator#Industrial Robots - MELFA

2026-02-01

Can robots fill the pharmaceutical supply gap?

Robotronic

Ogledate si video na YouTube
#Life Science#Industrial Robots - MELFA#Servo motors#Human-Machine Interfaces (HMIs) - GOT

2025-01-01

NEWMitsubishi Electric robot at Durable turns 25

Durable

EN
#Manufacturing#Industrial Robots - MELFA

2024-06-01

Industrial robots as an unusual measuring tool for testing radar sensors

Noffz GmbH

ENDE
#Automotive#Digitalisation#Industrial Robots - MELFA

2022-12-01

Robotics‑powered decorative coating from a single source

Singulus Technologies AG

DE
#Packaging#Material Handling#Servo motors#Programmable Controllers MELSEC#Industrial Robots - MELFA

2019-07-06

Robot duo cuts cakes & much more

Western Mechanical Handling (WMH)

DE
#Food & Beverage#Machine Building#AC Servos-MELSERVO#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA#Controllers

2018-11-01

Poka Yoke: Error-free manual workstations

Werkstatt Bremen - Martinshof

DE
Ogledate si video na YouTube
#Automotive#Material Handling#Controllers#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA